Início
  • Sites da Belimo
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
    Deutsch

    Français

    English

    中文

    Português

    Español

    Español

    Français

    Italiano

    Nederlands

    Türkçe

    Polski

    Norsk

    Suomalainen

    Svenska

    English

    Magyar

    Eesti keel

    Русский

    Latviski

    Lietuvių

    български

    language.el_GR

    עִברִית

    Română

    Slovenščina

    Slovenský

    Srpski

    Mакедонски

    Hrvatski

    Shqiptare

    Srpski

  • Sites da Belimo
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
  • DE FR EN 中文 PT ES ES FR IT NL TR PL NO FI SE EN HU ET RU LV LT BG EL HE RO SL SK SR MK HR SQ BA
Início
belimo_loxone_header_2

At the epicentre of intelligent
building automation.

  1. Início
  2. Destaques

  • Success story
  • Loxone as Belimo MP-Bus Partner
  • The Loxone Campus
Success story

A showcase project for learning and experiencing.

As a specialist for intelligent building automation solutions, Loxone has been supporting specialist planners, architects and building owners in the implementation of their building projects since 2009. With the help of its more than 25,000 partners worldwide, Loxone has already implemented more than 250,000 projects. Founded in 2009 in Kollerschlag, Austria, the company's mission is to use automation to create more energy-efficient, comfortable and safe buildings. Built in 2023 in the same place the company itself was founded, the purpose of the Loxone Campus is to make it possible to experience the building automation of tomorrow, today. The 15-hectare complex includes a hotel with a wellness centre, an auditorium, a restaurant, multiple office spaces and warehouses. It shows visitors what working and living may look like in the future. The entire heating, cooling and ventilation of the Loxone Campus was also designed to be automated and demand-controlled, which is why numerous communicative HVAC components from Belimo were used. Your advantages: Effortless integration into the building management system, energy-efficient operation and maximum comfort in the building. The Belimo Tree and Air interfaces enable seamless integration of the devices.

  • Reference – Loxone Campus, Austria (pdf - 2,32 MB)
  • Loxone Website
BUILDING TYPE         PROJECT            TRADES PRODUCTS
Multifunctional building      New Building Heating, ventilation, cooling Belimo Energy Valves with thermal energy meter
      6-way EPIVs
      PIQCVs
      Ventilation damper actuators
      Variable air volume
      Sensors

Intelligent energy efficiency and comfort.

"Our key requirements were to supply the extensive building stock of the Loxone Campus from a single technical centre, to meet the individual requirements of the variously used areas and at the same time to ensure that all areas were designed to be as flexible as possible for the future," says Jochen Sexlinger, Chief Technical Planner for the building project. To ensure optimum indoor air quality, most of the campus is CO2, humidity and temperature-controlled. At the same time, the building complex is intended to be operated as energy-efficiently as possible. All Belimo components are connected to the Loxone building automation system via MP-Bus for this purpose. Loxone has developed the Belimo Tree and Air interfaces for the seamless integration of Belimo products. Each interface enables the effortless connection of MP-Bus-compatible Belimo devices.

belimo_loxone_ev_orig
belimo_loxone_sexlinger
With the help of the Belimo Energy Valves and the 6-way characterised control valves, we can supply each consumer with the right energy as required and know exactly how much energy is flowing where.
Jochen Sexlinger
Chief Technical Planner, Sexlinger Consulting Engineering GmbH

Only as much energy as is needed.

The entire hydronic system in the main distribution system is designed to be electronically pressure-independent with Belimo Energy Valves. The Energy Valve provides all the important information that Loxone needs for energy monitoring and management. "We use the Belimo Energy Valve™ because it combines many functions in a single device – from metering to control to delta T management," says Jochen Sexlinger. "The Energy Valves allow us to monitor energy reliably. We can check the system at any time and optimise its operation". All hydronic balancing was done digitally, down to the smallest zone. This reduced the commissioning effort to a minimum.

The 80 hotel rooms in the Loxone Campus are equipped with ceiling induction units for heating and cooling, for which electronic pressure-independent 6-way valves (EPIV) from Belimo are used. Flow sensors from Belimo and sensors from Loxone measure the heating and cooling energy required in hotel rooms, saving energy when the rooms are unoccupied or when hotel guests are away. The ceiling induction units are installed in a two-pipe instead of a four-pipe version. Heat/cool changeover and control are implemented by a single 6-way valve. These solutions required fewer components, thus saving on both product and installation costs.

belimo_loxone_ahu_orig

The underfloor heating and cooling ensures a comfortable temperature in the office spaces at the Loxone Campus. The associated energy manifolds are equipped with pressure-independent characterised control valves (PICQV) from Belimo. The heat pump is operated using bad-point control: "We need a different amount of water for heating than for cooling, and, thanks to the manifold, we need to draw only so much energy as is actually required at any given time," says Jochen Sexlinger.

Multiple ventilation systems in the Loxone Campus ensure that all areas have comfortable temperatures, air humidity levels and CO2 concentrations. All ventilation systems are also equipped with ventilation damper actuators from Belimo. The ventilation of the Loxone campus is designed to use only as much outdoor air as is actually required, and to work with the recirculation air in the building, as part of overall energy efficiency requirements. Due to the reduced effort required for air conditioning, an optimal room climate can be ensured with low energy consumption, even when the outdoor air is dry in winter.

belimo_loxone_manifold_orig2

Efficient in every area.

The connection of all components to the building automation system of the Loxone Campus proved to be advantageous not only once the buildings had been put into operation, but also enabled extreme efficiency during the initial commissioning of the systems: "Whereas previously each room had to be set individually, here it was sufficient to program one of the hotel rooms and roll out the settings to all the others, thanks to the digital interfaces," recalls Jochen Sexlinger. "Thanks to intelligent building automation, such as we have here at the Loxone Campus, systems no longer need to be designed for full load, but can be operated in such a way that only the energy required is consumed. This would not have been possible with analogue systems," he concludes.

belimo_loxone_moser
By controlling and evaluating the Belimo Energy Valves, we benefit from maximum energy efficiency at the Loxone Campus
Thomas Moser
CEO Loxone Group
Loxone as Belimo MP-Bus Partner

Smart buildings require intelligent automation solutions that seamlessly integrate field devices. For this reason, Belimo has been working together with manufacturers of building automation solutions for many decades and supporting customers in the efficient implementation of their projects, including Loxone.

The cooperation with Loxone in the area of bus integration initially started with Modbus: Belimo created a Modbus library for the Belimo field devices. Loxone customers can use the corresponding templates unchanged or adapt them to specific projects. Later on, Loxone decided to implement the MP-Bus system, which supports the widest range of Belimo devices, allowing comprehensive flexibility in every project.

With Belimo Tree & Air, Loxone has created a gateway for both Loxone Tree and Loxone Air. Belimo supported Loxone throughout the entire implementation. The MP integration solution has also been implemented in the Loxone Campus and can therefore be put through its paces and optimised on an ongoing basis.


Directed to all higher-level systems

The MP-Bus® from Belimo was specially developed as a master/slave system for HVAC actuators. It allows up to eight different final control elements to be grouped together and connected to any higher-level system. 16 devices can be connected if only actuators of the latest design (e.g. ..-MPL) are used. Gateways and DDC controllers with an integrated MP interface serve as MP clients. There are no restrictions with respect to network topology. E.g. star, ring, line or mixed shapes are permissible.
 

belimo_loxone_server-clients

Easy wiring

The MP-Bus® uses a single installation cable, combining supply and communication in just three wires. It is very resistant to external interferences and requires no bus terminals.

belimo_loxone_interface

Designed for HVAC solutions

Loxone expert Johannes Bartnitzke and Andreas Marty, Head of Product Management EMEA at Belimo, will tell you all about the Belimo MP-Bus technology and its simple and rapid integration into Loxone home and building automation.
 

belimo_loxone_hetzendorfer
We have chosen to support Belimo's own MP-Bus as this allows us to support the widest range of Belimo devices and ensures maximum flexibility in every project. The native integration of Belimo into the Loxone Config makes it easier than ever to integrate Belimo devices into a building automation system. As a result, we offer not only the cheapest, but also the best solution.
Andreas Hetzendorfer
CPO, Loxone
The Loxone Campus

The Loxone Campus combines numerous fields of application in a single building complex. Intelligent building automation can be experienced first-hand in various scenarios.

Offices

The offices on the Loxone Campus cover 3,000 m2 and provide space for a total of 300 employees. Open-plan spaces with fixed workstations are complemented by bookable meeting rooms, soundproof phone booths, a lounge area and terraces for relaxation.

Pressure-independent characterised control valves from Belimo enable comfortable and energy-efficient heating and cooling of the offices using underfloor heating and cooling.
 

loxone_buero_manifold_orig

Hotel

The design hotel on the Loxone Campus has 80 rooms and two suites. In addition, a 500 m2 wellness area was built, which features an outdoor pool, two saunas, a gym and sunbathing areas.

Heating and cooling of the rooms takes place as required with ceiling induction devices. For these electronically pressure-independent 6-way control valves from Belimo were used, which ensure energy-efficient and reliable operation. The required energy is supplied as required, depending on occupancy and air quality.
 

belimo_loxone_hotel_valve_orig

Restaurant

The in-house restaurant is used all day by external guests, seminar participants and Loxone employees and can seat up to 600 people. If required, the restaurant can be connected to the adjoining auditorium using openable doors.

The air is fed into the restaurant and extracted in the kitchen. Pressure sensors from Belimo ensure that odours from the kitchen cannot overflow into the dining area or auditorium.
 

belimo_loxone_restaurant_ahu_orig

Auditorium

The auditorium of the Loxone Campus can be used for larger events, offering space for up to 600 people. The spacious hall can be used for concerts, events or lectures. In addition to featuring activities, it can also be used as part of the general catering facilities.

The auditorium is supplied by its own ventilation system, which feeds air underneath the grandstand. When the auditorium is connected to the restaurant, pressure sensors from Belimo enable optimum interaction between the ventilation systems in the two rooms.
 

belimo_loxone_auditorium_ahu_orig

Experience Zone

The Experience Zone in the Loxone Campus offers an interactive experience for visitors. The in-house cinema offers digital experience tours and enables a glimpse into the world of intelligent buildings. Visitors can learn more about the history of the company in the form of a miniature world. Other exhibits and interactive elements shall also be on offer, including gaming room.
 


Contate-nos Política de Privacidade Alterar as definições de privacidade
'+41 43 843 61 11
Se inscrever
BELIMO Automation AG, Brunnenbachstrasse 1, 8340 Hinwil, Suíça