Thermal Energy Meter Activation
Qualification for activation of Belimo's Thermal Energy Meters
The thermal energy meter meets the requirements of CSA C900 and EN1434 with type approval according to the Measurement Canada AV-2478-C and European Measuring Instruments Directive MID 2014/32/EU (MI-004).
Belimo's thermal energy meter is a multi-function device that can function as a heat meter, cold meter, or heat/cold meter. The meter can be installed in the system's supply or return. With the Belimo Assistant App, users choose the position during commissioning, known as activation. The authorized specialist who activates the thermal energy meter requires a Belimo Cloud account with additional authorization obtained through an online learning module. Activation of the thermal energy meter is carried out only once and is irreversible. It is essential to be attentive and mindful during activation. If activated incorrectly, the device will measure incorrectly and must be removed and replaced at the user's expense.