Complete offering of innovative HVAC field-devices
Belimo has earned the place of market leader by valuing ingenuity and craftsmanship and never resting on accomplishments. Very simply, we strive to build damper actuators, control valves and sensors that solve comfort and energy challenges, perform flawlessly and earn your trust through a long and productive life.
RetroFIT+
We understand buildings by offering solutions that maximise energy savings, improve system efficiency and elevate comfort levels.
Latest news
Customer-specific products
Custom-made products. Less effort, more profit.
Learn more
-
50th Annual General Meeting of BELIMO Holding AG Approves All Motions – March 25, 2025
-
Building Momentum – February 24, 2025
-
Double-Digit Organic Growth Validates Belimo's Long-Term Strategy – January 20, 2025
-
Proactive Succession Planning: James Furlong to Retire as Head of Group Division Americas and Member of the Executive Committee of the Belimo Group – December 10, 2024
-
Belimo strives for net-zero by 2050 with science-based targets – October 23, 2024
-
Belimo Continues Growth with Groundbreaking of New Logistics and Production Facility – October 1, 2024
-
More News
Belimo on Tour: Wir kommen zu Ihnen!
Ab April 2025 startet der Belimo-Van seine Roadshow-Tour in Österreich.
Mit Unterstützung unserer Fachleute erfahren Sie alles über unsere smarten Lösungen für mehr Komfort, Energieeffizienz und Sicherheit in Gebäuden sowie über deren Vorteile im Gebäudeentstehungsprozess und beim Unterhalt.
Belimo – leading in fire protection since 1978
Technology that saves lives
Fires represent the greatest potential threat to people and tangible assets in buildings. Efficient fire protection saves lives in times of danger, helps minimise property damage and secures the continued operation of companies.
Belimo fire protection products can be found in the following building applications:
- Motorised fire dampers for the formation of fire zones – they provide the best protection against the spread of fire and smoke through ducts
- Motorised smoke control dampers – they keep escape and rescue routes smoke-free in case of fire
- Actuators and sensors for pressure differential systems – they are used for smoke control in case of fire, e.g. in staircases in high-rise buildings
Success Story Loxone Campus, Austria
At the centre of intelligent building automation – A showcase project for learning and experiencing
Founded in 2009 in Kollerschlag, Austria, the company's mission is to use automation to create more energy-efficient, comfortable and safe buildings. Built in 2023 in the same place the company itself was founded, the purpose of the Loxone Campus is to make it possible to experience the building automation of tomorrow, today. The 15-hectare complex includes a hotel with a wellness centre, an auditorium, a restaurant, multiple office spaces and warehouses.
Innovations in comfort, energy efficiency and safety for buildings
For over 40 years, Belimo has successfully focused on the heating, ventilation, and air conditioning markets, providing quality solutions that will increase energy efficiency; reduce installation cost with the fastest delivery times in the industry. Our innovative products have always been designed to help achieve objectives better, faster, and more economically. Investing in new technology is key to our success, and Belimo will continue to offer products to help businesses succeed.
CESIM is the Belimo method to innovate building technology with sensors, valves, and actuators. CESIM ensures Comfort, Energy Efficiency, Safety for people and their property, while also ensuring easy installation, commissioning and reduced maintenance efforts.
Creating healthier indoor comfort with less energy
Buildings are responsible for 40% of global energy demand and greenhouse gas emissions. And because we spend up to 90% of our time indoors, they powerfully impact our comfort, health, and overall well-being. At Belimo, we have made it our mission to create healthier, more comfortable indoor environments that consume less energy. With a product portfolio naturally geared toward addressing several UN Sustainable Development Goals, we enable highly energy-efficient building automation and control systems (BACs) that cut the power requirements of HVAC solutions by up to 55%.
Basic requirements for HVAC systems for healthy indoor air quality
People spend approximately 90 percent of their time indoors and breathe 12,000 litres of air per day. It is therefore important to understand the powerful influence that indoor air quality has on our well-being. Belimo shares its deep insights into the effects of indoor humidity, VOC, and central air treatment systems and presents valuable suggestions for your health.
Belimo interviewed consulting engineers and experts in the ventilation sector around the world to identify the priorities when aspiring to create a healthy indoor air environment in a building. In the process, seven essential factors for ensuring healthy indoor air in non-residential buildings have emerged.
Learn more about:
Combine energy measure and control, certified thermal energy measurement and billing
The Belimo Energy Valve™ integrates energy metering, control, delta T management, and if required IoT-enabled billing in one device. It offers seamless and direct integration to the BMS or to IoT-based monitoring platforms, with IoT-based monitoring, performance improvement tools, and billing data. The two worlds of "energy control" and "certified thermal energy measurement and billing" are being united. Bringing together performance features to save you time and money.
HVAC air quality sensors for a healthy and efficient indoor climate
Our HVAC air quality sensors offer accurate measurements and an aesthetic and timeless design for architects, quick mounting for installers, easy commissioning with a smartphone for system integrators, and a comfortable and healthy room climate for occupants. With or without an ePaper touch display, they monitor and control multiple parameters necessary for indoor comfort and safety, including temperature, humidity, and CO2 levels. The room operating units with virtual displays allow complete and easy control without worrying about unauthorized access.
Ultrasonic flow sensor with glycol measurement
Trusted flow measurement is essential in maximising HVAC system efficiency and ensuring occupant comfort. Belimo’s new flow sensor utilises ultrasonic transit-time technology to provide accurate and repeatable flow measurements of water and water/glycol mixtures without drift in any HVAC application.
-
Multi-point wet calibrated to ensure accuracy and repeatability.
-
Patented temperature and glycol compensation logic eliminates manual calibration.
-
±2% accuracy of reading and ±0.5% repeatability ensure accurate and precise flow measurement.
Moving towards Building IoT with innovative products
Connectivity has always been a key feature of our products. Providing even better products with the right digital connection is our focus now and in the future.
The ecosystem of Belimo IoT devices enables flexible system integration through all common building automation communication protocols and Building IoT platforms. With the help of the additional IoT connection, buildings can be easily optimised, managed, and maintained.